This standard bit manipulation function contained in the <BIT_UTIL> library interchanges the value of the least significant Byte (LSB) and the most significant Byte (MSB) of the bit string applied at input IN.
Parameter |
Data type |
Description |
---|---|---|
IN |
WORD |
Input bit string |
OUT |
WORD |
Output bit string, values of LSB and MSB swapped |