CTUD / CTUD_S - Counter Up/Down

This counter function block counts up or down. In case of a rising edge at the input CU, CV is increased by one. In case of a rising edge at the input CD, CV decrements by one. If CV = PV, QU is set to TRUE. If CV = 0, QD is set to TRUE. If RESET = TRUE, the counter is initialized with 0. If LOAD = TRUE, the counter is initialized with PV. To enable the counting process, the inputs RESET and LOAD must be FALSE. Otherwise the counter will always be re-initialized.

The function block is available as standard function block CTUD and safety-related function block CTUD_S.

CTUD

Parameter

Data types

Description

CU

BOOL

If a rising edge is detected, CV is increased by one.

CD

BOOL

If a rising edge is detected, CV decrements by one.

RESET

BOOL

If TRUE, the counter is initialized with 0.

If FALSE, counting is enabled.

LOAD

BOOL

If TRUE, the counter is initialized with PV.

If FALSE, counting is enabled.

PV

INT

Preset value

QU

BOOL

TRUE if CV = PV

QD

BOOL

TRUE if CV = 0

CV

INT

Counter result

CTUD_S

Parameter

Data types

Description

CU

SAFEBOOL

If a rising edge is detected, CV is increased by one.

CD

SAFEBOOL

If a rising edge is detected, CV decrements by one.

RESET

SAFEBOOL

If TRUE, the counter is initialized with 0.

If FALSE, counting is enabled.

LOAD

SAFEBOOL

If TRUE, the counter is initialized with PV.

If FALSE, counting is enabled.

PV

SAFEINT

Preset value

QU

SAFEBOOL

TRUE if CV = PV

QD

SAFEBOOL

TRUE if CV = 0

CV

SAFEINT

Counter result

NOTE:

Function blocks have to be instantiated. Like variables, instances have to be declared before they can be inserted in a code body. Instances must be unique within the POU. In the following example, the instance name 'CTUD_S_1' is used.

Example for a safety-related function block declaration CTUD_S

Variables declarations

Local declarations:

Global declarations (I/O variables):

NOTE:

If you want to use the standard function block CTUD in your code worksheet, you have to select the data type 'CTUD' for the function block instance in the local variables worksheet. Accordingly, the data types 'BOOL' and 'INT' must be used instead of 'SAFEBOOL' and 'SAFEINT'.