System Requirements

Software requirements

To run Machine Expert – Safety, one of the following operating systems must be installed:

  • Microsoft Windows 11 (system locale English/USA or German/Germany) without beta releases of patches installed.

  • Microsoft Windows 10 (system locale English/USA or German/Germany) without beta releases of patches installed.

Hardware requirements

Machine Expert can be installed on a personal computer with the following hardware:

  • Processor Core 2 Duo or greater

  • RAM Memory 4 GB minimum, 8 GB recommended or greater

  • Hard disk 8 GB for typical and 15 GB for full software installation

  • Display 1280 x 1024 resolution or greater

  • Mouse or compatible pointing device

  • USB interface

  • Internet access