A variables worksheet contains one line for each variable or FB instance declaration. The properties of the declaration are contained in various grid columns.
For editing a particular property directly in the grid, left-click into the corresponding field and type the desired information. In some cases (e.g., for 'Type' and 'Usage') a drop-down combo box opens for selecting an entry.
Column |
Meaning |
||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|
Icon in first table cell |
The icon indicates the type of variable:
|
||||||||||
Name |
Name of the variable/instance. Machine Expert – Safety allows to use DIN qualifiers in IEC 61131 variable names. Rules for using DIN qualifiers According to the IEC 61131 standard, variable names can consist of letters, digits, and underscores. The identifier has to begin with a letter or an underscore. The use of any other character causes the compiler error "Illegal identifier". This naming convention has been expanded in Machine Expert – Safety in a way that IEC 61131 variable names may also contain DIN qualifiers:
Rules for using DIN qualifiers in IEC 61131 variable names
The variables grid indicates the following errors: Invalid names, multiple use. |
||||||||||
Online Value |
Online value of the variable read from the Safety Logic Controller or simulation during runtime (read-only). The column is only visible after the variables worksheet has been switched to online mode and if the grid line does not contain an FB instance declaration. When forcing or overwriting variables in debug mode, the forced/overwritten variable value is visible here. Forced values are shown on a pink background. Also refer to the related topics list below the table. |
||||||||||
Data type |
Data type of the variable. Data types determine what kind of value a variable can have. The data type defines the initial value, range of possible values, and the number of bits. Selection via drop-down combo box The 'Data type' combo box provides the elementary data types as well as all available FB types for selection.
|
||||||||||
Usage |
IEC 61131 variable declaration keyword and thus the type of the variable (e.g., input, output, symbolic variable). Selection via drop-down combo box In the 'Usage' combo box, the variable declaration keyword can be selected. The list is context-sensitive. Only keywords are provided for selection which are allowed for the present POU type.
NOTE:
In the global variables worksheet, the 'Usage' column is not visible because the keyword is set to VAR_GLOBAL by default. This column is not available in the global variables worksheet because the declaration keyword VAR_GLOBAL automatically applies to all global variables. |
||||||||||
Description |
User-defined comment. The comment entered here is also visible in the tooltip which appears when hovering the mouse over the respective object in the FBD/LD code. |
||||||||||
Terminal |
This column is only available in the global variables worksheet. It displays the name of the I/O terminal (physical address) to which the global I/O variable is assigned. After dragging a process data item into a code or variables worksheet, thus connecting the related terminal with a variable (see topic "Assigning variables to process data items"), the descriptive text of the connected process data item is visible in the 'Terminal' field of the global declaration. This terminal description is read from the device description file and cannot be edited. The variable grid indicates the following errors: Assignment to process data items which have been deleted in the mean time as well as multiple assignment. |
||||||||||
Init |
Initial value (only for variables, not for FB instances). According to IEC 61131-3 standard, initial values can optionally be assigned to variables. The initial value is applied when processing the variable for the first time during runtime. Rules for initializing variables
|
||||||||||
Confirm |
This column is only available in the global variables worksheet. It is only visible if a process data item has been modified. Left-click this checkbox to confirm the modified process data item. Background: This confirmation is required after modifying the bus structure in the Machine Expert 'Devices' window in a way that results in a different physical address of the related global I/O variable. (For example, by adding, deleting or replacing a device in the external bus configuration tool.)1 |
||||||||||
DIAG |
This flag is only available for local output variables (usage VAR_OUT) of the data type WORD. If selected, an implicit diagnostic is performed for this particular variable. Background: Safety-related firmware function blocks as well as user-defined FBs in a safety-related project may have a diagnostic output which allows polling of FB status information. This diagnostic information can be written to a reserved output buffer area (DQ buffer) while compiling and further processed, for example, using a diagnostic tool. Select the 'DIAG' flag to add the local output variable (FB output) to the DQ buffer. |
||||||||||
Feedback |
If this flag is set, the variable is considered as feedback variable. It can be used to program an implicit feedback in the safety logic.2 The 'Feedback' flag can only be set in combination with 'Usage = VAR' and 'Scope = Local'.
Further Information:
Refer to topic "Implicit feedbacks in FBD" for further information. |
1 |
Modifying the bus structure may result in a reassignment of the physical addresses of the devices. You must validate and, if necessary, reallocate the addresses of the related global I/O variables to ensure that the new addresses are correct and consistent. |
WARNING | |
---|---|
2 |
When programming implicit feedbacks, the safety logic may be constantly preempted by the updating of the feedback, which may result in a complex timing of your entire application. |
WARNING | |
---|---|