Output signal for controlling the connected contactors. If all the conditions have been satisfied, the S_EDM_Out output reflects the signal state at the S_OutControl input.
Data type: SAFEBOOL
As the enable signal is present at the S_EDM_Out output, this output is also referred to as the enable output.
Connection: Connect this output to the coils of the contactors to be monitored.
The enable signal may only control the process directly if this does not adversely affect the safety-related function.
WARNING | |
---|---|
Value |
Description |
---|---|
SAFETRUE |
The following conditions must be met:
|
SAFEFALSE |
This may be due to one of the following reasons:
|
Precise details of the behavior of the S_EDM_Out output in relation to the start-up inhibit are given in the following table:
Formal parameter |
Value |
Action |
Start-up inhibit |
Reset |
Enable output |
---|---|---|---|---|---|
S_StartReset |
SAFETRUE |
After function block activation/Safety Logic Controller start-up, the start-up inhibit is ... |
not active |
No action is required at Reset, ... |
- to switch the enable output S_EDM_Out to SAFETRUE if there is a valid input signal combination. - to exit the start-up inhibit. |
SAFEFALSE |
active |
Reset must be switched from FALSE to TRUE, ... |