FUNCTION_BLOCK BIT_AS_DWORD
Converts 32 input values of data type BOOL into an output value of the data type DWORD
InOut:
|
Scope
|
Name
|
Type
|
Comment
|
Input
|
B00
|
BOOL
|
Input bit 0
|
B01
|
BOOL
|
Input bit 1
|
B02
|
BOOL
|
Input bit 2
|
B03
|
BOOL
|
Input bit 3
|
B04
|
BOOL
|
Input bit 4
|
B05
|
BOOL
|
Input bit 5
|
B06
|
BOOL
|
Input bit 6
|
B07
|
BOOL
|
Input bit 7
|
B08
|
BOOL
|
Input bit 8
|
B09
|
BOOL
|
Input bit 9
|
B10
|
BOOL
|
Input bit 10
|
B11
|
BOOL
|
Input bit 11
|
B12
|
BOOL
|
Input bit 12
|
B13
|
BOOL
|
Input bit 13
|
B14
|
BOOL
|
Input bit 14
|
B15
|
BOOL
|
Input bit 15
|
B16
|
BOOL
|
Input bit 16
|
B17
|
BOOL
|
Input bit 17
|
B18
|
BOOL
|
Input bit 18
|
B19
|
BOOL
|
Input bit 19
|
B20
|
BOOL
|
Input bit 20
|
B21
|
BOOL
|
Input bit 21
|
B22
|
BOOL
|
Input bit 22
|
B23
|
BOOL
|
Input bit 23
|
B24
|
BOOL
|
Input bit 24
|
B25
|
BOOL
|
Input bit 25
|
B26
|
BOOL
|
Input bit 26
|
B27
|
BOOL
|
Input bit 27
|
B28
|
BOOL
|
Input bit 28
|
B29
|
BOOL
|
Input bit 29
|
B30
|
BOOL
|
Input bit 30
|
B31
|
BOOL
|
Input bit 31
|
Output
|
X
|
DWORD
|
Output value
|
|