ScriptTextualObject

class

ScriptTextualObject.

ScriptTextualObjectMarker

Bases: object

All tree objects get amended with this marker.

Version added

3.5.6.0

has_textual_declaration

Gets a value indicating whether this ScriptObject has a textual declaration part.

Return type

bool

Returns

True if it has a textual declaration; otherwise False.

has_textual_implementation

Gets a value indicating whether this ScriptObject has a textual implementation part.

Return type

bool

Returns

True if it has a textual implementation; otherwise False.

class

ScriptTextualObject.

ScriptTextDocument

Bases: object

Interface for a text document, as it is used e. G. in textual declaration and implementation parts.

Line endings ('\n', '\r', '\r\n') are normalized to '\n'. Lines do not include the line ending character. The first character has offset 0, the first line has lineno 0.

Version added

3.5.6.0

length

Gets the length of the text document in bytes.

Return type

int

linecount

Gets the number of lines in the current text document.

Line endings ('\n', '\r', '\r\n') are normalized to '\n'. Lines do not include the line ending character. The first line has lineno 0.

Return type

int

text

Gets the complete text as a string.

Return type

str

get_line

lineno

Gets the line with the specified lineno.

Lines do not include the line ending character. The first line has lineno 0.

Parameters

lineno (int) -- The line number.

Return type

str

Returns

The line.

get_text

length

offset=None

lineno=None

lineoffset=None

Gets the text.

 WARNING

The original C# function that is called with this method contains 2 overloads. It is strongly advised to pass all arguments with their respective keywords. offset, lineno and lineoffset are not actually optional, they just aren't required in every overload. Pass them if your overload needs them!

get_text(self, offset, length) (1/2)

Gets the text at the specified offset.

Return type

str

get_text(self, lineno, lineoffset, length) (2/2)

Gets the text at the specified lineno.

Parameters

lineoffset (int) -- The offset within the line.

Return type

str

replace_line

lineno

line

Replaces the complete line with the specified line number with the new text.

This method retains the position info of the text lines which are not modified.

append

text

Appends the specified text at the end of the buffer.

This method retains the position info of the text lines which are not modified.

Parameters

text (str) -- The text.

insert

text

offset=None

lineno=None

lineoffset=None

Insert text.

 WARNING

The original C# function that is called with this method contains 2 overloads. It is strongly advised to pass all arguments with their respective keywords. offset, lineno and lineoffset are not actually optional, they just aren't required in every overload. Pass them if your overload needs them!

insert(self, offset, text) (1/2)

Inserts the text at the specified offset.

This method retains the position info of the text lines which are not modified.

insert(self, lineno, lineoffset, text) (2/2)

Inserts the text at the offset of the specified line.

This method retains the position info of the text lines which are not modified.

Parameters

lineoffset (int) -- The offset within the line.

Return type

str

remove

length

offset=None

lineno=None

lineoffset=None

Remove text.

 WARNING

The original C# function that is called with this method contains 2 overloads. It is strongly advised to pass all arguments with their respective keywords. offset, lineno and lineoffset are not actually optional, they just aren't required in every overload. Pass them if your overload needs them!

remove(self, offset, length) (1/2)

Removes the text at the specified offset.

This method retains the position info of the text lines which are not modified.

remove(self, lineno, lineoffset, length) (2/2)

Removes the text at the specified offset of the specified line.

This method retains the position info of the text lines which are not modified.

Parameters

lineoffset (int) -- The offset within the line.

replace

new_text=None

newtext=None

length=None

offset=None

lineno=None

lineoffset=None

Replace text.

 WARNING

The original C# function that is called with this method contains 3 overloads. It is strongly advised to pass all arguments with their respective keywords. No argument is actually optional, they just aren't required in every overload. Pass them if your overload needs them!

replace(self, offset, length, newtext) (1/3)

Removes the text at the specified offset.

This method retains the position info of the text lines which are not modified.

Parameters

newtext (str) -- The new text.

replace(self, lineno, lineoffset, length, newtext) (2/3)

Removes the text at the specified offset of the specified line.

This method retains the position info of the text lines which are not modified.

Parameters
  • lineoffset (int) -- The offset within the line.

  • newtext (str) -- The new text.

replace (self, new_text) (3/3)

Sets the specified new text.

This method erases the position info (used for bookmarks etc).

Parameters

new_text (str) -- The new text.

class

ScriptTextualObject.

ScriptObjectWithTextualDeclaration

Bases: ScriptTextualObject.ScriptTextualObjectMarker

Accessor interface for textual declaration parts.

Version added

3.5.6.0

textual_declaration

Gets the textual declaration.

Return type

class

ScriptTextualObject.

ScriptObjectWithTextualImplementation

Bases: ScriptTextualObject.ScriptTextualObjectMarker

Accessor interface for textual implementation parts.

Version added

3.5.6.0

textual_implementation

Gets the textual implementation.

Return type