ScriptTextListObject

class

ScriptTextListObject.

ScriptTextListMarker

Bases: object

Marker object to check whether an ScriptObject is a textlist object.

Version added

3.5.11.0

is_textlist

Gets a value indicating whether this ScriptApplicationMarker is a textlist.

Return type

bool

Returns

True if it is a textlist; otherwise False.

class

ScriptTextListObject.

ScriptTextListObject

Bases: ScriptTextListObject.ScriptTextListMarker

ScriptObjects which are a textlist object are extended with this interface.

Version added

3.5.11.0

addlanguage

language

Adds a new language to the text list.

If the language already exists, it is not added twice.

removelanguage

language

Removes a new language to the text list.

rows

Gets the collection of the rows currently configured within this textlist.

languagecount

Gets the current number of languages in this textlist.

Return type

int

getlanguage

index

Returns the language with the given index.

Parameters

index (int) -- The index of the language to return.

Raises

ArgumentOutOfRangeException -- Thrown when the given index is not in the valid range.

Return type

str

updatetextids

Only for global textlist.

Calls the command 'Update Visualization Text IDs' for this textlist. This command updates all inconsistent IDs in a static text list.

checkids

Only for global textlist.

Calls the command 'Check Visualization Text IDs' for this textlist. This command checks whether the ID of a text list entry in the project is correct and reports the result.

removeunusedids

Only for global textlist.

Calls the command 'Remove Unused Text List Entries' for this textlist. This command checks whether a text list entry in the project is used as static text. If not, CODESYS removes it from the text list.

importfile

importfile

Like in import/export dialog: The file can contain text list entries both for the global text list and for text lists.

importreplacementfile

importfile

Like in import/export dialog: The replacement file contains replacements for the global text list.

Parameters

importfile (str) -- Name and path of a file of type csv.

export

exportfile

Like in import/export dialog: exports all the texts from all the text lists in the current project.

class

ScriptTextListObject.

ScriptTextListRow

Bases: object

A row within an ScriptTextListObject.

Version added

3.5.11.0

id

The identification of the row.

Return type

str

defaulttext

The default text entry in this row.

Return type

str

setlanguagetext

language

text

Sets the text in the row, for a defined language.

Parameters
  • language (str) -- The languagename, which defines the language entry, to use.

  • text (str) -- The text to set for this language.

Raises

ArgumentOutOfRangeException -- Thrown when the language does not yet exist in the textlist.

Return type

bool

Returns

True if the text could be set, otherwise False.

setdefaulttext

defaulttext

Sets the defaulttext in this row.

Parameters

defaulttext (str) -- The defaultext to set for this row.

Return type

bool

Returns

True if the text could be set, otherwise False.

languagetextcount

Gets the current number of languagetexts in this row.

Return type

int

languagetext

index

Gets the languagetext.

Parameters

index (int) -- The index of the languagetext to return.

Raises

ArgumentOutOfRangeException -- Thrown when the given index is not in the valid range.

Return type

str

Returns

The language text.

class

ScriptTextListObject.

ScriptTextListItemsCollection

Bases: list

The items currently managed by the textlist object.

Version added

3.5.11.0

add

id

defaulttext

Adds a new row to the current textlist.

Parameters
  • id (str) -- The id to assign to the newly inserted row. Must not yet be existing.

  • defaulttext (str) -- The default text.

Return type
Returns

The newly created ScriptTextListRow.

remove

id

Removes the ScriptTextListRow with the given id.

Parameters

id (str) -- The id of the item to remove.

Raises

KeyNotFoundException -- Thrown when no entry with the given id exists.

class

ScriptTextListObject.

ScriptTextListObjectContainer

Bases: object

Projects and Application Objects are extended with this interface.

Version added

3.5.11.0

create_textlist

name=None

Creates a new textlist object in the current context (either application or project global).

Parameters

name (str) -- The name of the new textlist object. In case of None, a default name will be generated.

Raises

ArgumentException -- Thrown when a textlist with the given name already exists within the current context.

Return type
Returns

The newly created textlist object.

get_global_textlist

Returns the global textlist object or creates a new one if not yet existing.

Typically this method can be called on projects only. Only in case of special customizations of the programming system, it is allowed to call this on an application too.

Return type
Returns

The global textlist.

has_global_textlist

Checks whether there is already a global textlist in the current location.

Only in case of special customizations of the programming system, it is allowed to call this on an application too.

Raises

InvalidOperationException -- Thrown when called on applications when this is not allowed.

Return type

bool