|
Input
|
xEnable
|
BOOL
|
TRUE
|
Enable function
|
|
AR_ID
|
DWORD
|
CommFB.Constants.INVALID_ID
|
ID of the Application Relation ( = Connection) that has to be checked.
|
|
Index
|
DINT
|
0
|
Index of the expected submodule. Range [0 - ExpectedSubmoduleCount - 1].
|
|
Output
|
xValid
|
BOOL
|
|
The displayed data is valid. This means the specified Index and AR-ID are valid.
|
|
ExpectedSubmoduleCount
|
DINT
|
|
Number of expected submodules within the specified Connect- req.
|
|
ExpectedSubmodule
|
ExpSubmodule
|
|
Data of the Expected Submodule that is currectly selected by the input Index.
|
|
xModuleDiff
|
BOOL
|
|
There is some mismatch in the submodule configuration
|
|
ModuleState
|
ModuleState
|
16#FFFF
|
ModuleState that will be returned to the controller.
|
|
ARInfo
|
SubmoduleState_ARInfo
|
|
AR releated information that will be returned to the controller.
|
|
IdentInfo
|
SubmoduleState_IdentInfo
|
|
Identification releated infiormaton that will be returned to the controller.
|