IOReset

 

IOReset

General

Type

EF

Offline editable

Yes

Devices supporting the parameter

OnBoard I/O

Traceable

Functional Description

The parameter affects the resetting of the OnBoard I/O outputs. The value must be configured in offline mode. In the case of a reset or a download of the projects, the setting used is that which is saved in the boot project.

Any online change of the parameter IOReset is discarded during the actions Reset warm, Reset cold and Download.

Value

Data type

Meaning

no reset / 0

DINT

The outputs are not reset after the program has been downloaded.

after download / 1

DINT

The outputs are reset after the program has been downloaded.

after download or prg. Reset / 2

DINT

The outputs are reset after a download or a reset of the program.

after download, prg. Reset or prg. stop / 3

DINT

The outputs are reset after a download, a reset, or a stop of the program.

See also ...

oDigital Output Group

oResetValue