Type: |
Method |
Available as of: |
V2.14.0.0 |
Versions: |
Current version |
This chapter provides information on:
Get the configuration data for the EcoStruxure Machine Expert Twin communication of the Lexium P Robot.
By calling the method, the configuration data for the OPC UA data structure of the Lexium P Robot can be read.
Output |
Data type |
Description |
---|---|---|
q_etDiag |
General, library-independent statement on the diagnostic. A value not equal to ET_Diag.Ok corresponds to a diagnostic message. |
|
q_etDiagExt |
POU-specific output for the diagnostic. q_etDiag = ET_Diag.Ok -> Status message q_etDiag <> ET_Diag.Ok -> Diagnostic message |
|
q_sMsg |
STRING[80] |
Event-triggered message that gives additional information on the diagnostic state. |
q_stData |
DTC.ST_ConfigDataRobotPSeries |
Read out the data that have been configured to emulate this robot in EcoStruxure Machine Expert Twin. |
q_etDiag |
q_etDiagExt |
Enumeration value |
Description |
---|---|---|---|
OK |
OK |
0 |
Successful |
ExecutionAborted |
RobotNotInitialized |
89 |
The robot is not initialized. |
ExecutionAborted |
DigitalTwinConfigDataNotSet |
128 |
Configuration data for EcoStruxure Machine Expert Twin have not been set. |
Enumeration name: |
RobotNotInitialized |
Enumeration value: |
89 |
Description: |
The robot is not initialized. |
Issue |
Cause |
Solution |
---|---|---|
Reading the EcoStruxure Machine Expert Twin configuration parameter was unsuccessful. |
The robot is not initialized. |
Verify that the robot has been initialized successfully. |
Enumeration name: |
DigitalTwinConfigDataNotSet |
Enumeration value: |
128 |
Description: |
Configuration data for EcoStruxure Machine Expert Twin have not been set. |
Issue |
Cause |
Solution |
---|---|---|
Reading the EcoStruxure Machine Expert Twin configuration parameters was unsuccessful. |
The EcoStruxure Machine Expert Twin configuration parameters have not been set |
Verify that the method SetDigitalTwinConfigData has been called successfully. |