LConTo (FB)

FUNCTION_BLOCK LConTo EXTENDS TimingControlledBehaviourModelBase IMPLEMENTS ILConTo

Base implementation of a PLCopen Level Controlled Behavior Model (see: ILConTo)

For use, this block should be extended and the specific inputs and outputs must be supplemented. The output eErrorID of the application-specific enum type ERROR must be added.

InOut:

Scope

Name

Type

Comment

Input

xEnable

BOOL

TRUE: Activates the defined operation FALSE: Aborts/resets the defined operation

udiTimeOut

UDINT

Max. operating time for executing [µs], 0: No operating time limit

Output

xDone

BOOL

TRUE: Ready condition reached

xBusy

BOOL

TRUE: Operation is running

xError

BOOL

TRUE: Error condition reached