FUNCTION_BLOCK LConC EXTENDS BehaviourModelBase IMPLEMENTS ILConC
Base implementation of a PLCopen Level Controlled Behavior Model (see: ILConC)
For use, this block should be extended and the specific inputs and outputs must be supplemented. The output eErrorID of the application-specific enum type ERROR must be added.
InOut: |
|