FUNCTION MemFill : BOOL
Function fills all bytes of a memory block with the value "byFillValue". In case of success, the function will return “TRUE”. Only if "MemoryBlock" is set to "0", the initialization will not be carried out and the function will return "FALSE".
InOut: |
|