FUNCTION GetBusAlarm : BOOL
This function returns if the CAN chip is in Bus Alarm state. In this state sending and receiving messages is not possible. A Bus Alarm can be reset by ResetBusAlarm which leads to a re-initialization of the CAN chip. Diagnostic Information can be also read by GetDiagnosis.
InOut: |
|