SET_MSB

This standard bit manipulation function contained in the <BIT_UTIL> library writes the value applied at input MSB to the most significant Byte of the bit string applied at input DATA.

Parameter

Data type

Description

MSB

BYTE

Value to be written to the MSB of DATA

DATA

WORD

Input bit string to be modified

OUT

WORD

Output bit string with modified written MSB