AND / AND_S - AND connection

This bitwise Boolean function realizes a logical AND integration of the operands connected to the input parameters. It is available as standard function AND and safety-related function AND_S.

AND

Parameter

Data types

Description

IN1

ANY_BIT

Input value

IN2

ANY_BIT

Input value

OUT

ANY_BIT

Output value

AND_S

Parameter

Data types

Description

IN1

ANY_SAFEBIT

Input value

IN2

ANY_SAFEBIT

Input value

OUT

ANY_SAFEBIT

Output value

NOTE:

Input parameters can be duplicated.

NOTE:

All parameters must have the same data type.