Machine Expert > V2.1 > Logiciel > Bibliothèques, Modèles et Exemples > Bibliothèques > CODESYS Libraries > CmpUserMgr Implementation Library Documentation > CmpUserMgr > Functions > Objecthandling > UserMgrObjectRemove (FUN)

UserMgrObjectRemove (FUN)

FUNCTION UserMgrObjectRemove : RTS_IEC_RESULT

Removes an object from the user management and all its children

InOut:

Scope

Name

Type

Comment

Return

UserMgrObjectRemove

RTS_IEC_RESULT

Error code
  • ERR_OK: Object could be removed

  • ERR_PARAMETER: Invalid object handle

Input

hObject

RTS_IEC_HANDLE

Handle to object