IOL_Error (STRUCT)

TYPE IOL_Error : STRUCT

This datastructure contains the decoded error information of a failed IOL_CALL-FB execution

For details see:

[1] PI Specification, IO-Link Integration, Part 1, Version 1.0, December 2007, Order No. 2.812

[2] IO-Link Community, IO-Link Interface and System, V1.1.2, July 2013

InOut:

Name

Type

Comment

PortError

IOL_PortError

IOL-Call Error codes, see [1]

ErrorCode

IOL_ErrorCode

IO-Link Error codes according AL_Read/ AL_Write services; see [2].

AdditionalCode

IOL_AdditionalCode

IO-Link Error codes according AL_Read/ AL_Write services; see [2].