DiagnosisSeverity (ENUM)

TYPE DiagnosisSeverity :

The severity expresses how urgent maintenance is demanded to cure a specific diagnosis:

Attributes:

qualified_only

InOut:

Name

Comment

Undefined

(data is not init.)

Normal

Normal operation, all OK.

Advice

Advice means normal operation; however, the process delivers an advice for the user.

MaintenanceRequired

Maintenance required means that maintenance should be done in a near future.

MaintenanceDemanded

Maintenance demanded demands maintenance as fast as possible.

Fault

Fault means immediate action; the channel is no longer working.