ConfigError (ENUM)

TYPE ConfigError :

Attributes:

qualified_only

InOut:

Name

Initial

Comment

OK

0

Success

INVALID_ID

1

The provided ID is not valid

INVALID_STATE

2

The current device status does not allow update of the value

INVALID_DEVICE_TYPE

3

Operation not possible for this type of device

INDEX_NOT_FOUND

4

INVALID_DATA_LEN

5

NOT_IMPLEMENTED

16#FF

This driver does not implement the config update