ERROR (ENUM)

TYPE ERROR :

CIP Errors (0-255) and library specific errors (256-x)

Attributes:

qualified_only

InOut:

Name

Initial

Comment

NO_ERROR

0

Service was successfully performed by the object specified.

CONNECTION_FAILURE

16#1

A connection related service failed along the connection path.

RESOURCE_UNAVAILABLE

16#2

Resources needed for the object to perform the requested service were unavailable

INVALID_PARAM_VALUE

16#3

See Status Code 0x20, which is the preferred value to use for this condition.

PATH_SEGMENT_ERROR

16#4

The path segment identifier or the segment syntax was not understood by the processing node. Path processing shall stop when a path segment error is encountered.

PATH_DESTINATION_UNKNOWN

16#5

The path is referencing an object class, instance or structure element that is not known or is not contained in the processing node. Path processing shall stop when a path destination unknown error is encountered.

PARTIAL_TRANSFER

16#6

Only part of the expected data was transferred.

CONNECTION_LOST

16#7

The messaging connection was lost.

SERVICE_NOT_SUPPORTED

16#8

The requested service was not implemented or was not defined for this Object Class/Instance.

INVALID_ATTRIBUTE_VALUE

16#9

Invalid attribute data detected.

ATTRIBUTE_LIST_ERROR

16#A

An attribute in the Get_Attribute_List or Set_Attribute_List response has a non-zero status.

ALREADY_IN_REQUEST_STATE

16#B

The object is already in the mode/state being requested by the service

OBJECT_STATE_ERROR

16#C

The object cannot perform the requested service in its current mode/state.

OBJECT_ALREADY_EXISTS

16#D

The requested instance of object to be created already exists.

ATTRIBUTE_NOT_SETTABLE

16#E

A request to modify a nonmodifiable attribute was received.

PRIVILEGE_VIOLATION

16#F

A permission/privilege check failed

DEVICE_STATE_ERROR

16#10

The device’s current mode/state prohibits the execution of the requested service.

REPLY_DATA_TOO_LARGE

16#11

The data to be transmitted in the response buffer is larger than the allocated response buffer

FRAGMENTATION_OF_VALUE

16#12

The service specified an operation that is going to fragment a primitive data value, i.e. half a REAL data type.

NOT_ENOUGH_DATA

16#13

The service did not supply enough data to perform the specified operation.

ATTRIBUTE_NOT_SUPPORTED

16#14

The attribute specified in the request is not supported.

TOO_MUCH_DATA

16#15

The service supplied more data than was expected.

OBJECT_DOES_NOT_EXIST

16#16

The object specified does not exist in the device.

SERVICE_FRAGMENTATION_SEQUENCE_NOT_IN_PROGRESS

16#17

The fragmentation sequence for this service is not currently active for this data.

NO_STORED_ATTRIBUTE_DATA

16#18

The attribute data of this object was not saved prior to the requested service.

STORE_OPERATION_FAILURE

16#19

The attribute data of this object was not saved due to a failure during the attempt.

ROUTING_FAILURE_REQUEST_PACKET_TOO_LARGE

16#1A

The service request packet was too large for transmission on a network in the path to the destination. The routing device was forced to abort the service.

ROUTING_FAILURE_RESPONSE_PACKET_TOO_LARGE

16#1B

The service response packet was too large for transmission on a network in the path from the destination. The routing device was forced to abort the service.

MISSING_ATTRIBUTE_LIST_ENTRY_DATA

16#1C

The service did not supply an attribute in a list of attributes that was needed by the service to perform the requested behavior.

INVALID_ATTRIBUTE_VALUE_LIST

16#1D

The service is returning the list of attributes supplied with status information for those attributes that were invalid.

EMBEDDED_SERVICE_ERROR

16#1E

An embedded service resulted in an error.

VENDOR_SPECIFIC_ERROR

16#1F

A vendor specific error has been encountered. The Additional Code Field of the Error Response defines the particular error encountered. Use of this General Error Code should only be performed when none of the Error Codes presented in this table or within an Object Class definition accurately reflect the error.

INVALID_PARAMETER

16#20

A parameter associated with the request was invalid. This code is used when a parameter does not meet the requirements of this specification and/or the requirements defined in an Application Object Specification.

WRITE_ONEC_VALUE_OR_MEDIUM_ALREADY_WRITTEN

16#21

An attempt was made to write to a write-once medium (e.g. WORM drive, PROM) that has already been written, or to modify a value that cannot be changed once established.

INVALID_REPLY_RECEIVED

16#22

An invalid reply is received (e.g. reply service code does not match the request service code, or reply message is shorter than the minimum expected reply size). This status code can serve for other causes of invalid replies.

BUFFER_OVERFLOW

16#23

The message received is larger than the receiving buffer can handle. The entire message was discarded.

MESSAGE_FORMAT_ERROR

16#24

The format of the received message is not supported by the server.

KEY_FAILURE_IN_PATH

16#25

The Key Segment that was included as the first segment in the path does not match the destination module. The object specific status shall indicate which part of the key check failed.

PATH_SIZE_INVALID

16#26

The size of the path which was sent with the Service Request is either not large enough to allow the Request to be routed to an object or too much routing data was included.

UNEXPECTED_ATTRIBUTE_IN_LIST

16#27

An attempt was made to set an attribute that is not able to be set at this time.

INVALID_MEMBER_ID

16#28

The Member ID specified in the request does not exist in the specified Class/Instance/Attribute

MEMBER_NOT_SETTABLE

16#29

A request to modify a non-modifiable member was received

GROUP_2_ONLY_SERVER_GENERAL_FAILURE

16#2A

This error code may only be reported by DeviceNet Group 2 Only servers with 4K or less code space and only in place of Service not supported, Attribute not supported and Attribute not settable.

UNKNOWN_MODBUS_ERROR

16#2B

A CIP to Modbus translator received an unknown Modbus Exception Code.

ATTRIBUTE_NOT_GETTABLE

16#2C

A request to read a non-readable attribute was received

INSTANCE_NOT_DELETABLE

16#2D

The requested object instance cannot be deleted

SERVICE_NOT_SUPPORTED_FOR_SPECIFIED_PATH

16#2E

The object supports the service, but not for the designated application path (e.g. attribute). NOTE: Not to be used for any set service (use General Status Code 0x0E or 0x29 instead)

TIME_OUT

16#100

Request timed out.

INTERFACE_MISSING

IEtherNetIPService is not implemented.

REMOTE_CALL_FAILED

No physical connection.

NULL_POINTER

Wrong input value NULL.

INVALID_DATA_SIZE

Size of data unacceptable.

WRONG_INTERFACE_VERSION

Version missmatch. Device implements not the same version of interface for the called method.

NO_MEMORY

Not enough memory

UNKNOWN_ERROR

An unknown error occured.

ABORTED

Service was aborted