Apply_Attributes (FB)

FUNCTION_BLOCK Apply_Attributes EXTENDS BaseService

This function block is used for calling the "Apply_Attributes" service of a specific instance of a CIP object. As a result, the attributes that were previously set with "Get_Attribut_Single" or "Get_Attribut_All" are adopted and saved by the adapter.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

itfEtherNetIPDevice

IEtherNetIPService

EtherNet/IP Device which implements the EtherNet/IP Services interface

BaseService

eClass

CIPClass

Class which shall perform the service

BaseService

dwInstance

DWORD

Instance which shall perform the service (0: Class level, 1..x: Instance level)

BaseService

Output

eError

ERROR

Error (0-255: CIP Error; 256-x: Library Error)

BaseService