ITimingControlled (ITF)

INTERFACE ITimingControlled EXTENDS __SYSTEM.IQueryInterface

Used for IActionProvider instances whose behaviour model either requires a udiTimeLimit or a udiTimeOut input. It can also require both of these inputs. Because of this the related BehaviourModel instance is using an ITimingController instance.

This decorator is referenced by the following interfaces: IETrigTl (ITF) | IETrigTo (ITF) | IETrigTlTo (ITF) | IETrigATl (ITF) | IETrigATo (ITF) | IETrigATlTo (ITF) | ILConTl (ITF) | ILConTo (ITF) | ILConTlTo (ITF) | ILConTlC (ITF)