RCVREC (FB)

FUNCTION_BLOCK RCVREC

A Field Device can receive an acyclic process data record from a Host Controller or a Supervisor (The Host may use the WRREC function block).

The application of a programmable field device is informed about this request and can receive the data using the RCVREC function block.

This function blocks contains the methods to check, receive and acknowledge a process data record.

All aspects of receiving a process data record may use one function block instance, the different methods are distinguished using the MODE input.

IF a data record is received (with MODE=1 OR MODE=2), the NEW output indicates that the data record is stored in the variable given AT the RECORD parameter.

If the function block refuses to accept the data record, the CODE1 input sets the Error Code 1, and the CODE2 input sets the Error Code 2 of the negative response.

If an error occurred, the ENO=0 indicates an error and the STATUS output contains the error code.

Note

The application program of the Field Device shall acknowledge the received request, otherwise the Host Controller will get a timeout error or the device stack will send a negative response.

Code-Example

PROGRAM ReceiveData
VAR
    recvData: CommFB.RCVREC;
    data : ARRAY [0..64] OF BYTE;

    recvAll: CommFB.RCVREC;
    param1 : ARRAY [0..7] OF BYTE;
    param2 : ARRAY [0..7] OF BYTE;
END_VAR

// Variant 1: receive data for a specific slot:
recvData.EN := 1;
recvData.F_ID := CommFB.SUBSLOT_ID(EN := TRUE, PN_Device.DeviceID, 2, 1);   // get ID of Slot 2 of the specified device
recvData.MLEN := SIZEOF(data);
recvData.RECORD := ADR(data);
recvData (MODE := CommFB.RCVREC_MODE.RECEIVE_BY_SLOT);      // receive data and write it to RECORD
IF recvData.NEW THEN
    IF(recvData.INDEX = 10) THEN
        // ...process and opt. check received data
        recvData(MODE := CommFB.RCVREC_MODE.POS_RESPONSE);  // send pos. response to host
    ELSE
        recvData(MODE := CommFB.RCVREC_MODE.NEG_RESPONSE, CODE1 := CommFB.ErrorCode1_RW.Invalid_index);  // signal error to host
    END_IF
END_IF

// Variant 2: check for any request and then (opt.) receive it in a second step
// MODE := 0  = CommFB.RCVREC_MODE.CHECK
// MODE := 1  = CommFB.RCVREC_MODE.RECEIVE
// MODE := 3  = CommFB.RCVREC_MODE.POS_RESPONSE
// MODE := 4  = CommFB.RCVREC_MODE.NEG_RESPONSE
recvAll(EN := TRUE, MODE := 0);     // check for new data
IF(recvAll.NEW) THEN                // received data
    IF(recvAll.SLOT = 1 AND recvAll.INDEX = 100) THEN
        recvAll(MODE := 1, MLEN := SIZEOF(param1), RECORD := ADR(param1));      // get data
        recvAll(MODE := 3);     // pos. response
    ELSIF(recvAll.SLOT = 3 AND recvAll.INDEX = 200) THEN
        recvAll(MODE := 1, MLEN := SIZEOF(param2), RECORD := ADR(param2));      // get data
        recvAll(MODE := 3);     // pos. response
    ELSE
        recvAll(MODE := 4, CODE1 := CommFB.ErrorCode1_RW.Invalid_slot_or_subslot);     // signal error to host
    END_IF
END_IF
InOut:

Scope

Name

Type

Comment

Input

EN

BOOL

The function is invoked by EN=1.

MODE

UINT

Function specifier, see RCVREC_MODE

F_ID

DWORD

Slot / subslot to filter the data records to receive

MLEN

UINT

Maximum length of a data record to receive

CODE1

BYTE

Reason for negative response. (see ErrorCode1_RW)

CODE2

BYTE

Reason for negative response. (0 or user specific)

RECORD

POINTER TO BYTE

Received data record. Shall be at least of MLEN byte

Output

ENO

BOOL

Function enabled

NEW

BOOL

New data record received

STATUS

DWORD

Field Device interface status

SLOT

UINT

Slot the record is received for

SUBSLOT

UINT

Subslot the record is received for

INDEX

UINT

Index of the received data record

LEN

UINT

Length of the received data record