ReverseBitsInDWORD (FUN)

FUNCTION ReverseBitsInDWORD : DWORD

Function returns the DWORD "dwInput" with a reversed bit-order.

Example:

dwInput = 16#01020304 = 2#00000001 00000010 00000011 00000100
->
MEM.ReverseBitsInDWORD(dwInput) = 16#20C04080 = 2#00100000 11000000 01000000 10000000
InOut:

Scope

Name

Type

Comment

Return

ReverseBitsInDWORD

DWORD

function returns a DWORD with reveresed bit-order of "dwInput"

Input

dwInput

DWORD

DWORD to reverse