FUNCTION_BLOCK Hysteresis_DINT
This function block will set the output variable to TRUE, if the integral value
is smaller than an integral lower bound
It will set the Boolean output variable to FALSE, if the input value
exceeds the integral upper bound
.
If
lies between the lower and upper bound, the value of the output will rest unchanged by the module.
| InOut: |
|