DirCopy (FB; Prefix fildcp)

FUNCTION_BLOCK DirCopy EXTENDS CBM.ETrig

This function block copies the contents of the source directory to the destination directory Nonexisting destination path will be created. Depending of the parameters, all subdirectories and its content will be copied too, and existing files will be overwritten. NOTE: Empty direcories will be copied if xRecursive is TRUE.

InOut:

Scope

Name

Type

Comment

Input

sDirNameDest

CAA.FILENAME

destination directory name

sDirNameSource

CAA.FILENAME

source directory name

xRecursive

BOOL

TRUE: all subdirectories and their contents are copied, FALSE: subdirectories are omitted

xOverWrite

BOOL

TRUE: existing files are overwritten, FALSE: existing files are left untouched

Output

eError

ERROR

Local library error ID (0: no error; 5101: time out)