IsSendingActive (FUN)

FUNCTION IsSendingActive : BOOL

This function specifies whether the CAN hardware is busy sending CAN messages or whether further messages are stored and waiting to be sent.

InOut:

Scope

Name

Type

Comment

Return

IsSendingActive

BOOL

FALSE if the sending queue is empty and the CAN hardware is actually not transmitting a message.

Input

hDriver

CAA.HANDLE

handle of CAN interface

peError

POINTER TO ERROR

optional pointer to error enum