SMC_DetermineCuboidBearing (FB)
FUNCTION_BLOCK SMC_DetermineCuboidBearing
This function block will determine the position of a cuboid (corner mark, edge alignment) in the space in dependence of 6 (3/2/1) points given:
For detailed information of transformation modules see the survey on Coordinate Transformations.
InOut:
Scope |
Name |
Type |
Initial |
Comment |
Input |
A1 |
SMC_Vector3D |
First of three points that are located on the surface A of a cube and do not lie on a common line. |
|
A2 |
SMC_Vector3D |
Second of three points that are located on the surface A of a cube and do not lie on a common line. |
||
A3 |
SMC_Vector3D |
Third of three points that are located on the surface A of a cube and do not lie on a common line. |
||
B1 |
SMC_Vector3D |
First of two points that are located on another cube surface B adjacent to A. The projection of this point on surface A may not coincide with the projection of B2. |
||
B2 |
SMC_Vector3D |
Second of two points that are located on another cube surface B adjacent to A. The projection of this point on surface A may not coincide with the projection of B1. |
||
C1 |
SMC_Vector3D |
Point on a further cube surface adjacent to A and B |
||
Output |
M |
SMC_Vector3D |
Common corner point of cube surfaces A, B and C |
|
vAB |
SMC_Vector3D |
Unit vector on edge line between A and B with start point M |
||
vBC |
SMC_Vector3D |
Unit vector on edge line between B and C with start point M |
||
vCA |
SMC_Vector3D |
Unit vector on edge line between A and C with start point M |
||
bError |
BOOL |
Signals, that an error has occurred within the function block |
||
nError |
WORD |
0 |
Error description:
|