This function of the CAA_Memory.library looks for the first occurrence of " byValue " in "MemoryBlock".
It will return 0, if „byValue“ cannot be found. Else, the position of the first occurrence will be returned.
|
pMemoryBlock |
DWORD |
Address of memory area MemoryBlock |
|
uiLengthBlock |
UINT |
Size of area MemoryBlock in byte |
|
byValue |
BYTE |
Byte to be retrieved |
|
MEM.FindByte |
UINT |
Position of first occurrence, if existent; 0 else. |
Example:
abyMemoryBlockA : ARRAY[0..9] OF BYTE := 0,1,2,3,4,5,6,7,8,9 ;
->
MEM.FindByte(ADR(abyMemoryBlockA),10,5) = 6