MBM.XChgDelete (FUN)

 

(CAA_MemBlockMan.Library)

All resources which are allocated by the Exchange identifed by hXChg, get deallocated. It will be detected automatically, via which method (MBM.XChgCreateH oder MBM.XChgCreateP) the Exchange had been created.

Input:

hXChg

CAA.HANDLE

Handle of the Exchange to be deleted.

Output:

eError

MBM.Error

Error description.