Onboard I/O
General
The OnBoard I/O has to be added to the drive. To do so, right-click the drive in the Devices tree and select Add device... from the context menu.
What Is in This Part?
This part contains the following chapters:
oName
oState
oDiagClass
oDiagCode
oDiagSource
oDiagMsg
oDiagExtMsg
oIO0_Mode, IO1_Mode
oIO4_Mode, IO5_Mode
oFailSave
oIOReset
oTouchprobe Inputs
oDigital Outputs
oDigital Inputs