Type |
AF |
Devices supporting the parameter |
Virt. Master Encoder |
Traceable |
No |
Displays the actual velocity of the virtual master encoder in units/s.
A unit is defined using the parameter FeedConstant.
RefVelocity specifies the reference velocity of the virtual master encoder.
If Enable is "off / 0", the velocity of the encoder is set to 0.