Type |
AD |
Devices supporting the parameter |
Incremental Encoder Input |
Traceable |
Yes |
When zero track detection is enabled, this bit indicates whether a zero track has been detected.
Value |
Data type |
Meaning |
---|---|---|
false / 0 |
BOOL |
No Zero Track detected. |
true / 1 |
BOOL |
Zero Track detected. |
NOTE: When a zero track is detected, the Position of the incremental encoder input is set to 0. The detection of a zero impulse has no effect on the Position parameter of any incremental encoder simulation output that may be present.